Author Topic: Opening up pages with a full view of the frame  (Read 4351 times)

Offline njuelsgaard

  • PLUS+1 Novice
  • *
  • Posts: 1
  • Karma: +0/-0
    • ALMACO Home Page
Opening up pages with a full view of the frame
« on: May 26, 2016, 03:47:31 PM »
Hi, Plus+1 noob here. Is there a setting or an easy way to have a full view of the entire frame/titlebox of a page when you enter it? I can't seem to find any easy answer in the manual or the forum.

Thanks!

Offline Daniel

  • PLUS+1 Expert
  • ****
  • Posts: 74
  • Karma: +6/-0
Re: Opening up pages with a full view of the frame
« Reply #1 on: May 27, 2016, 10:54:37 AM »
Hello njuelsgaard

No, not to the frame. When entering a page it will automatically zoom so all content on the page will fit to the screen, but this does not count the frame around as a "content". This is the same as when using the Home key on the keyboard to zoom "Fit page".
However, if there are no items at all inside the page, it will zoom to the page frame when entering, but I would guess you normally have something in the page.

The zooms available are found in under View --> Zoom. There are also some settings available for Zoom in Setup --> Options.


Best regards
Daniel
PLUS+1® Helpdesk
PLUS+1® Help Desk Team

Offline jashom1

  • PLUS+1 Expert
  • ****
  • Posts: 78
  • Karma: +6/-0
Re: Opening up pages with a full view of the frame
« Reply #2 on: May 31, 2016, 07:03:34 AM »
If you place a rectangle outside the boarder it will then zoom to view all including the page boundary.  I too find it a pain sometimes where it's default zoom level is in too far.

Cheers,

John.