Author Topic: Adding Hardware - Error 302  (Read 5689 times)

Offline Keithang

  • PLUS+1 Developer
  • ***
  • Posts: 20
  • Karma: +0/-0
Adding Hardware - Error 302
« on: July 27, 2015, 11:49:23 AM »
Hi,

When I create a new project in Plus+1 GUIDE 7.1.12, and try to open up a controller, I get the following error:

ERROR 302 [PLUS1_IDE] INTERNAL: UNEXPECTED EXCEPTION WITH MESSAGE: {No Open project}.

I am using the evaluation version, ultimate Beginner and would like to get to know the program whilst training online.

Thomas

  • Guest
Re: Adding Hardware - Error 302
« Reply #1 on: July 27, 2015, 01:20:47 PM »
Hello!

Please make sure that you have full admin rights when you install and use the program. You could try and right click on on the PLUS+1 GUIDE icon and Run as Administrator.
It is also recommended to use the latest version from our website. Hope this helps.

If the problems remains please contact our help desk directly for more support.
http://powersolutions.danfoss.com/products/plus-1-guide/plus-1-support-and-training/

Thomas

Offline bryantmorris

  • PLUS+1 Expert
  • ****
  • Posts: 51
  • Karma: +0/-1
Re: Adding Hardware - Error 302
« Reply #2 on: August 30, 2017, 06:28:21 AM »
I was having the same problem but I found running the program in Windows 10 as admin helped fixed the issue.