Author Topic: Guide 7.0.8 ?  (Read 5235 times)

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Guide 7.0.8 ?
« on: November 13, 2014, 11:00:10 AM »
Hi,
I have seen, there is a new Guide 7.0.8.
I am using the version 7.0.7.
What is the difference?
I can't find a readme file. The last readme file is 7.0.7. There is no readme 7.0.8.

Thanks.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 103
  • Karma: +2/-0
    • Getman Corporation
Re: Guide 7.0.8 ?
« Reply #1 on: November 13, 2014, 01:22:49 PM »
This is off the release notes within 7.0.8

VERSION 7.0.8 (September 2014)
-New Features and Functionality (see the GUIDE User Manual for more detailed information)
-Important Advisory—Potential User Issues
(No changes from 7.0.7)
-What is Fixed
[P100003069] An incorrect checksum calculation made it impossible to download some applications to
SC-controllers. This has now been fixed.
[P100003093] Text lists in large screen definitions could in some cases result in a compile error. This
has now been fixed.
[P100003094] It was not possible to use several instances of a screen definition. This has now been
fixed.
[P100003108] Scaled and rotated image lists got the wrong insertion point. This has now been fixed.
[P100003131] The position of an image list containing a rotated image was not stored correctly. This
has now been fixed.
[P100002967] In some cases, importing a screen definition would cause the vector based screen editor
to crash. This has now been fixed.
2

Offline Daniel

  • PLUS+1 Expert
  • ****
  • Posts: 74
  • Karma: +6/-0
Re: Guide 7.0.8 ?
« Reply #2 on: November 13, 2014, 02:40:52 PM »
Hi

Here are the release notes for GUIDE 7.0.8.

Best regards
Daniel
PLUS+1® Help Desk Team

bgtwuk

  • Guest
Re: Guide 7.0.8 ?
« Reply #3 on: November 14, 2014, 12:22:36 AM »
Has any one else had trouble opening the Data files or API spec sheets when using 7.0.7?

Bgtwuk

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Guide 7.0.8 ?
« Reply #4 on: November 14, 2014, 08:14:20 AM »
Yes , there was sometimes trouble with opening pdf-Files.
But now , it works, I don't know why.

Sometimes , I can't open the manual.
When I have opened another PDF, I can't open Danfoss PDF's starting from guide, and vice versa.

I will watch it and tell you exactly.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung