Author Topic: Max size for a text list?  (Read 1764 times)

Offline BBarry

  • PLUS+1 Developer
  • ***
  • Posts: 14
  • Karma: +0/-0
Max size for a text list?
« on: August 29, 2022, 03:53:02 PM »
Hey Brilliant People!
Looking in the manuals I could not find this. For the DM430.

Is there a size limit on the Text Lists? (outside of the u8 0-255) limit on the Active Index?

Like total string char limit?

I am planning to use a text list for alarm history page and need to know if I am limited to the number of alarms (text strings) I may have in a list?

Warmest regards,

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 275
  • Karma: +26/-1
Re: Max size for a text list?
« Reply #1 on: August 30, 2022, 11:18:40 AM »
Hello BBarry,

As far as I could find after asking the PLUS+1 Team there are no direct limitations for the text list.
The type of the signal, memory and how much time you have to add alarm texts.
And I believe that the Active Index is not limited to a U8.

I hope it helped
Best regards,
Tor
PLUS+1® SW PAE Team

Offline BBarry

  • PLUS+1 Developer
  • ***
  • Posts: 14
  • Karma: +0/-0
Re: Max size for a text list?
« Reply #2 on: August 30, 2022, 04:07:36 PM »
That did help. Thank You!