Recent Posts

Pages: 1 ... 8 9 [10]
91
PLUS+1 Service Tool / Re: *.p1log-journal filename extension
« Last post by Tor on February 08, 2022, 10:00:41 AM »
Hi gregbosma,

Sorry about the late response, but I saw that you got help from the PLUS+1 Helpdesk.
I thought I write something here as well if someone else run into this.

According to the developers the ".p1log-journal" is a temporary file and cannot be opened by PLUS+1 Service Tool. The actual log file always have the ".p1log" extension.
I guess something went wrong during the log and a ".p1log" file wasn't created.


Have a nice day.
92
Displays / Re: Signal Type Mismatch for HMIs
« Last post by acmall on February 01, 2022, 09:17:59 AM »
The input type for the screen definition can be changed in the Screen Editor. In the Screen Manager window scroll down to the bottom where you will find Input and Output. Expand Input and select the input you want to change then change the type in the inspector.

If the Screen Manager window is not visible you can show it using the icon circled in the attached image.
93
Displays / Signal Type Mismatch for HMIs
« Last post by ZanInno on February 01, 2022, 07:13:26 AM »
I have a number of signals coming into an HMI / DM430.  I often get messages like the following:

[CHPARGU1] Type mismatch: Signal {Input.Eng0.Eng0_CoolTemp_110} has type {S16} in the drawing and type {S8} in the {Screen Definition} interface

I am deleting / re creating text definitions to try and fix it - The tags are simply received via CAN and displayed on a screen. How are the tags defined in the text definition?  The tags that are coming in are S16.  Not used anywhere else in the program. 

Thanks
94
Controllers / Re: use MC50 and IOX24 together
« Last post by topal on January 31, 2022, 07:03:40 PM »
Hello, acmall

you are the king, it"s work very fine

thank you very much

Pat
95
PLUS+1 Service Tool / *.p1log-journal filename extension
« Last post by gregbosma on January 31, 2022, 03:36:59 PM »
A service tech sent me a Plus+1 log file with the filename extension ".p1log-journal" and I'm unable to open it using Plus+1 Service Tool.  Until now, every log file I've received had a ".p1log" filename extension, without the "-journal" added onto it. How can I get this ".p1log-journal" file open and look at data?
96
Controllers / Re: use MC50 and IOX24 together
« Last post by acmall on January 31, 2022, 09:07:02 AM »
In the program you posted you have connected the input form the IO module C1p09 to a CAN transmit message with ID 0x200 that you are transmitting on CAN_1. You have C1p37 connected to a CAN receive message with ID 0x200 also on CAN_1. This will not work as you can not transmit a message and simultaneously receive it on the same CAN port.

To have C1p37 go high in response to an input on the IO module C1p09 you just need to connect the DigIn from C1p09 on the IO module to the DigOut of C1p37.
97
Controllers / Re: use MC50 and IOX24 together
« Last post by topal on January 30, 2022, 09:09:19 PM »
Hello,

i confirm, on IOX24 red led sparkles, green led flashes quickly at power on and after the green led blink at 1 hz

i have configured my iox with Service Tool

RX id 300
TX id 180
baudrate 250K
N1 0
NET 1
Address mode 1
Mask 0

can you help me

Thank

Pat
98
Controllers / Re: use MC50 and IOX24 together
« Last post by FluidPowerTom on January 30, 2022, 06:04:03 PM »
Can you confirm that per Marbek's image you set Address Mode to 1 and set the N1 value to 0?

What are the two LED's doing on your IO module?  Both should be blinking rapidly (much faster than 1 Hz).
99
Controllers / Re: use MC50 and IOX24 together
« Last post by topal on January 30, 2022, 02:58:58 PM »
Hello,

I post my program because even with the explanations of Marbek_Elektronik

it does not work !

I tried everything but I have to miss something that I don't see

it's simple, however, what I want is by putting the C1P09 input of IOX24 to 12 volts that facing it, switch the C1P37 output of my MC50 to the high state to be able to light a bulb

the exercise seems simple but I can't do it

can someone take a look at my program and tell me where i made the mistake

thank you

Pat
100
Displays / Re: DM430 new hardware file
« Last post by niteRider on January 28, 2022, 06:00:09 PM »
bummer... must have missed that one.  Thanks!
Pages: 1 ... 8 9 [10]