Recent Posts

Pages: 1 [2] 3 4 ... 10
11
Controllers / Re: Controller Output diode
« Last post by acmall on May 12, 2022, 08:58:44 AM »

The diode being optional is mentioned on page 4 of this document, although it does not specify any particular controller type.

https://assets.danfoss.com/documents/53526/BC152886483485en-000501.pdf

12
Controllers / Controller Output diode
« Last post by macbahi on May 11, 2022, 08:15:18 PM »
Hi!!

I read the recirculating diode across the relay coil is optional.

Please how can I know if my controller has some output with this option. 

What documentation please.

Thank you very much

with best regards
13
Controllers / Re: POU Input output
« Last post by macbahi on May 10, 2022, 05:58:50 PM »
Thank you Tom
14
Controllers / Re: POU Input output
« Last post by FluidPowerTom on May 09, 2022, 07:59:01 PM »
In this case the variable names on the input and output busses for the POU will need to be INT1, INT2, and Out2. 

What you can do is don't connect the input bus and output bus from the POU to your main busses.  Instead, for example, connect your input signal 'Signal1' by itself to the input bus of the POU, and then rename it on that bus as INT1.  So you'll have just the green wires going to the input bus and output bus of the POU.  Does that make sense?
15
Controllers / POU Input output
« Last post by macbahi on May 09, 2022, 05:31:53 PM »
HellO,

I use POU  Structured text function as using in video #21.  It's working.

But my idea it's to use this function many times.  It can be used to calculate any things as simple example: Sum of 2 variables.

Function Sum
VAR_INPUT
     INT1  INT
     INT2  INT
VAR_OUPUT
     Out2  INT

Code
   Out2 := INT1 + INT2;


But When I call from call POU I must make the input and output as in function. In my example function are INT1, INT2 and Out2.
If other name variable  as data1,  data2  and Sum1 problem with compilation.

Please have idea how we can use POU structured text call without using the same name as input and output in function.

Thank you very much

Cordialy
Mac bahi
16
General controls / Re: Red and Green information about all module
« Last post by macbahi on May 09, 2022, 04:51:02 PM »
Hello!!

thank you for your replay

sincerely
Mac bahi
17
Controllers / Re: output shared
« Last post by topal on May 08, 2022, 08:36:10 AM »
Hello,

i used this way and it works

thank you

Pat
18
PLUS+1 Telematics Hardware / Re: CS500: No current config was found
« Last post by dlewis on May 06, 2022, 01:29:34 PM »
Well, it's working again.  I did nothing special except wait a day and attempted to download again.  This time it worked.
19
This is all good news, so thanks for following up on this.  Concerns are alleviated!
20
Hello,

To clarify for everybody, it's possible to update the CS100 firmware with the PLUS+1 Service Tool.  It was a misunderstanding from Helpdesk that it didn't work.

We will try to get a confirmation regarding the PIB, since the date from Microsoft has been changed. I hope a new PIB will be sent out.
I will post the information as soon as I get it.


Have nice day
Pages: 1 [2] 3 4 ... 10