Author Topic: OutpuMode modification needed  (Read 15031 times)

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 127
  • Karma: +1/-0
OutpuMode modification needed
« on: November 14, 2024, 07:53:58 PM »
Hello,

In the past I have change InputMode to use 2 mode in the same input and same project.  It's done with help from Sir Matt_Eng and Sir Tor (thanks another time).
You can see my topic link in the end of this message.
 
But now I want to change the OutputMode.  Because I want to use Output C2P03  one time as Sink Mode 2 and one time as PWM mode 3.   Please is it possible to do that?
My problem is in Output configuration page, Digout must one time connected to False and one time not.  And DutyOut one time connected to 0 (U16) and one time not connected.
Please have you any idea to do that.

Thanks in advance
Hamid
https://www.plus1forum.danfoss.com/index.php?topic=1525.msg5109#msg5109

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 127
  • Karma: +1/-0
Re: OutpuMode modification needed
« Reply #1 on: November 14, 2024, 08:53:32 PM »
Hello again,

It's done compilation without using switch I just put both DigOut and DutyOut not connected.

but I am not sure if this way is safe.

I will give the news soon.

With best regards

Offline Lukey

  • PLUS+1 Expert
  • ****
  • Posts: 73
  • Karma: +8/-0
Re: OutpuMode modification needed
« Reply #2 on: November 15, 2024, 01:25:02 AM »
It is possible to change the output mode during operation.

I have successfully change between output mode 1 & 2.
This allowed me to drive a PNP and NPN (Sink and Source) wired relays from the 1 output.
That gave me 2 outputs from the 1 output, excellent for controlling a 2 way DCV for example.