Hello,
Please I need more information about output mode 0, 1 2 and 7.
Output mode 0 is push/pull so if DigOut is set to 0 the output will be GND
if DigOut is set to 1 the output will be Vcc
Output mode 1 is push/pull so if DigOut is set to 0 the output will be Floating signal. Are you agree?

if DigOut is set to 1 the output will be Vcc
Output mode 2 is push/pull so if DigOut is set to 0 the output will be Floating signal or GND? I am not sûre what is?
if DigOut is set to 1 the output will be GND.
Mode 3 is not is not clear for me when The output is set logic 0. The outpout is foating or GND.
Concerning output mode 7 I never use it. Please Could you give more information with schematic will be more appreciated.
I need when an output when is OFF, The output is floating and when the Output is ON the Output will be GND.
Thank you very much.
With best regards