91
Controllers / Re: Where to Start
« Last post by acmall on June 19, 2023, 04:17:21 PM »Also note that most of the displays can be connected to via USB for programing. Upload times to the display are a lot quicker when connected via USB especially if you have a program that uses a lot of images or other files. The display can also act as the gateway to connect to any other Danfoss controller that is connected to any of the displays CAN ports.