Author Topic: Icons for Module viewer, ServiceTool and Guide  (Read 4186 times)

Offline Fredrick

  • PLUS+1 Developer
  • ***
  • Posts: 27
  • Karma: +4/-0
Icons for Module viewer, ServiceTool and Guide
« on: October 05, 2020, 06:49:30 PM »
When I normally working in GUIDE i have the Module Viewer and ServiceTool running as well and I would like to have bigger differents between the icons in the taskbar.
Now there is no different between the Module viewer and GUIDE makeing it hard to click on the right one when I need to change between them.

Is there possible to change this somewhere?

« Last Edit: October 05, 2020, 06:57:15 PM by Fredrick »

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 278
  • Karma: +27/-1
Re: Icons for Module viewer, ServiceTool and Guide
« Reply #1 on: October 06, 2020, 12:10:37 PM »
Hi Fredrick,

If you want a quick fix for this, you can change the windows setting to show labels in the task bar. Then it shows what program is open.
But, if you are anything like me and want a "clean look", there is not much you can do.

I will ask the developers if this is a bug or a wish for future release of PLUS+1, because I agree with you.


Thank You
Best regards,
Tor
PLUS+1® SW PAE Team