Author Topic: Low voltage  (Read 5214 times)

paterianus

  • Guest
Low voltage
« on: January 14, 2011, 10:56:43 PM »
Is there a defined hardware shutdown for the Plus1 controller in low voltage situations or must the user program this failure mode?

Offline Thomas

  • PLUS+1 Guru
  • *****
  • Posts: 128
  • Karma: +6/-0
    • PLUS+1 support pages
Re: Low voltage
« Reply #1 on: January 17, 2011, 06:28:45 AM »
Hi!

The hardware will run between 9 and 36 volt in most controllers and displays but there is no functionality for low voltage situations. You can create that function yourself by monitor the voltage on the power pin.

Best regards // Thomas