Author Topic: Is there a CANOpen Master module  (Read 4703 times)

power4

  • Guest
Is there a CANOpen Master module
« on: November 05, 2013, 10:33:22 PM »
I am trying to connect a MC050 or MC024 controller to some motor controllers which are working as CANOpen Slave nodes on a CAN bus. The MC controller will be a CANOpen Master node, which needs to initialize the slaves and send TPDO message. I noticed the built-in CAN module in the controller is very generic, so, I just want to ask if there is a library or module directly for CAN master node.

Thanks.

Offline Neil

  • PLUS+1 Expert
  • ****
  • Posts: 96
  • Karma: +2/-0
Re: Is there a CANOpen Master module
« Reply #1 on: November 07, 2013, 07:30:45 PM »
Hi Power4.

no there isn't you have to build the logic into the controllers yourself.
I have succesfully run Danfoss FC electric motor drives from a DP610.

regards Neil.