Author Topic: Error: No valid PLG file available  (Read 5046 times)

Maxim

  • Guest
Error: No valid PLG file available
« on: May 13, 2013, 02:11:01 PM »


I've set up this a network with a plus1 controller and a DP250-00-00-04-00-00 Display.
How can I solve this error?

Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 98
  • Karma: +2/-0
Re: Error: No valid PLG file available
« Reply #1 on: May 13, 2013, 02:19:26 PM »
Hi Maxim

It looks like your program download was interupted, and now the display is running a bootloader program.
I would try and download your program again, in such a case.
If it keeps on being interupted, then check your CAN-bus network. 2 times 120 ohms that gives a total resistance of 60 ohm.

I hope this helps a bit.

Jakob

Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 98
  • Karma: +2/-0
Re: Error: No valid PLG file available
« Reply #2 on: May 13, 2013, 02:57:12 PM »
Another possibility is that you have a "unstable" CAN-bus interface.
I tried that with a CG150, that kept giving me this error.

So if you have a spare interface, that would be something to try.

Maxim

  • Guest
Re: Error: No valid PLG file available
« Reply #3 on: May 16, 2013, 10:26:24 AM »
Thank you, problem solved!