Author Topic: application log not enable  (Read 5137 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
application log not enable
« on: September 24, 2012, 06:36:43 PM »
Hello there,

Look for some reason the application log menu is not enable in my plus1 guide 5.0 software, I pull down the menu but the " define application log ares page" and the "define application log file".

I have opened an application for a DP600 so the menu should be able to use.

Does anyone knows what is needed to enable such feature?

I appreciate

Regards,


Offline mebib

  • PLUS+1 Developer
  • ***
  • Posts: 18
  • Karma: +0/-0
Re: application log not enable
« Reply #1 on: September 24, 2012, 10:19:57 PM »
Hello Pinias

The DP600 is not supporting the application log. Check for the DP600LX, it will have 16MB of application log memory.

Regards

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
Re: application log not enable
« Reply #2 on: September 26, 2012, 08:41:29 PM »
Mebid,

alright data storage is not the same that data logging.

thanks