PLUS+1 Tools > PLUS+1 Service Tool

how to monitor the system value

(1/1)

daifuku chan:
Which botton to monitor the system?And read the value of the output?  THANKS   :-\ :-\

Jakob:
The "hotkey" for those functions are shown in the dropdown menu's at the top of the screen.
Start logging = F5

Scan connected system = F8

Upload parameters = F2       (Read parameters from ECU)
Download parameters = F4   (Write parameters into ECU)

Im not sure if this answers your question, tho.

Navigation

[0] Message Index

Go to full version