PLUS+1™ Hardware > PLUS+1™ Compliant Hardware

MPCAN Receiver for IK2 Transmitter

(1/1)

sfl_cntrl:
I've downloaded the available documentation for the IK2 transmitter and MPCAN Receiver, and do not find any information on how to interface this device to a controller via CAN bus. Where can I find information on the signals being sent from the IK2 and how this information is framed at the receiving MPCAN?

For example, if I move Joystick A what can I expect to receive at the MPCAN, and is it located at Byte 1, 2, 7 etc?? Is there a CAN database file available for this hardware?

Navigation

[0] Message Index

Go to full version