Author Topic: DP720 Import Data  (Read 5740 times)

Offline Emerson Zaionc

  • PLUS+1 User
  • **
  • Posts: 9
  • Karma: +0/-0
DP720 Import Data
« on: September 14, 2017, 06:16:32 PM »
Hello guys.

I would like to know if the DP720 Display is possible to use the front USB to import information into the HMI. Example: Put a USB bar code reader in front of the HMI and be able to import this information into the HMI.

Or put a pendrive with a .txt file, read it and insert it into the respective fields .txt example:

1; -29.998555; -51.201119; 3000; 20; 50; 50;
1; -29.998555; -51.201119; 2000; 20; 60; 40;
1; -29.998555; -51.201119; 1000; 20; 70; 30;
1; -29.998555; -51.201119; 500; 20; 85; 15;
//
2; -27.653372; -52.247508; 2000; 25; 30; 70;
2; -27.653372; -52.247508; 1500; 25; 20; 80;
2; -27.653372; -52.247508; 1000; 25; 20; 80;
2; -27.653372; -52.247508; 500; 25; 10; 90;
//

Example of how they would look after being imported into the HMI:

Image attached.

I would like your opinion on this, whether it is possible or not. If you have some examples of how to perform this operation I would be very grateful.

Thank you in advance for your help.