PLUS+1 User Forum

PLUS+1 Hardware => PLUS+1 CS Hardware => Topic started by: pinias on March 25, 2022, 08:38:53 PM

Title: CS100 CONFIGURATION AT PORTAL
Post by: pinias on March 25, 2022, 08:38:53 PM
Hi Guys,

this is the first time I will be using a CS100, still waiting for the device but in the mean time I tried to do a simple  configuration for it on the PLUS1 Connect portal.

when trying to do it I had few errors, is that becuase the device is not added on the PLUS 1 Connect portal yet?

see screen shots, basically it does not accept the CAN ID I want to work with, not sure what multiplier means, it asks for ID Mask but it is 11 bit only CAN ID.

does anyone can advise about

thank you
Title: Re: CS100 CONFIGURATION AT PORTAL
Post by: pinias on April 22, 2022, 06:05:37 PM
Just an update about

we are 2 administrators of the portal, so both should be able to create and modify the configuration files, however for some reason just my colleage can do that, if I try to do it, it seems to work until I hit the save/create button, basically it saves no any changes I made. we have compared all adminstrator settings and both are the same..kind of odd this issue.

Regards