PLUS+1 User Forum
PLUS+1 Tools => PLUS+1 Service Tool => Topic started by: deyan.dimitro on January 16, 2019, 12:43:27 PM
-
Hello,
i have a temperature sensor connected in ECU. Input pin is C1p27.Ohm and unit is Ohm. I must not change nothing in GUIDE Project File.
Can i get the information from this pin but in degrees in Service Tool?
I have Danfoss temperature sensor table.
-
No, not really. All the elements only offer linear scaling, some with an offset. I can think of two options:
- Insert that image into the service tool for manual ohms-temperature cross-referencing, or
- break the table into sections that are nearly linear, within your tolerance, and put in "panel" objects for each of the ranges, using the "hide component" feature to select a valid range of ohms for which to display the particular panel. Then insert a linearly converted standard log object in each panel for that range.