PLUS+1 User Forum
PLUS+1 Tools => PLUS+1 Service Tool => Topic started by: alwilgus on October 24, 2017, 10:02:24 AM
-
I have an old CG150 (not the CG150-2). I installed it using the update drivers. CAN King can read my sensor with it. But the Service Tool does not find my MC012-110 controller. The download page have no controller in the drop down. Is it my CG150, the way I installed it, the way the Service Tool is setup, the MC012-110? This is my first attempt at using Danfoss. I built the lhx using GUIDE and it compiled. Any help would be appriciated. I am version 9.1 for the GUIDE and Service Tool.
-
I also have the older version of the CG150 and have not had any issues with MC088-015, MC50-110, MC38-010 controller or DP610 & DP720 displays.
If CANKing is working with your CG150 it would suggest that it is working ok.
Check the following:-
- In the status bar at the bottom of the service tool screen does it display a green circle and say Connected?
- In the status bar at the bottom of the service tool screen does it display CG150 #0 (Channel0)?
- Is your controller displayed in the ECU list in the system navigator?
Alastair
-
I have an MC012-110 but used MC012-010 in GUIDE. Made the change and every works now. (Everyone has that first project as a nube, but I am now on to the next project) :D