Author Topic: E270: Invaild data in file.....  (Read 25159 times)

Offline PARK HAN SOO

  • PLUS+1 Novice
  • *
  • Posts: 3
  • Karma: +0/-0
E270: Invaild data in file.....
« on: August 08, 2024, 11:55:14 AM »
Any body knows what this error means, and how to solve it?
I can't open the service tool file. :-X :-X :-X

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 203
  • Karma: +37/-1
Re: E270: Invaild data in file.....
« Reply #1 on: August 09, 2024, 08:49:55 AM »
This could be cased by this issue.

[P100007144] P1D files saved in 2024.2.4 could not be opened by a user of older Service Tools that also used an old version of P1 Base.

If you open the Update Center it should pop up a message that there is new version of the Update Center. This will also update P1 Base.

Offline PARK HAN SOO

  • PLUS+1 Novice
  • *
  • Posts: 3
  • Karma: +0/-0
Re: E270: Invaild data in file.....
« Reply #2 on: August 09, 2024, 09:31:32 AM »
It opens on my computer, but not on other computers with the same version of the service tool installed.

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 203
  • Karma: +37/-1
Re: E270: Invaild data in file.....
« Reply #3 on: August 09, 2024, 09:54:16 AM »
It is not the version of the Service Tool that you are using to open the file that causes the issue I posted, it is the version of P1 Base.

We had the exact same issue you are describing and it was resolved by updating the Update Center which also updates P1 Base. After doing this the file could be opened in the same version of the Service Tool that was previously giving the error.

 

Offline PARK HAN SOO

  • PLUS+1 Novice
  • *
  • Posts: 3
  • Karma: +0/-0
Re: E270: Invaild data in file.....
« Reply #4 on: August 12, 2024, 07:36:31 AM »
Thank for your reply.
I solved the problem. Thank you. :D :D :D :D