Author Topic: NOT enable signal for screen object  (Read 3071 times)

Offline BBarry

  • PLUS+1 Developer
  • ***
  • Posts: 14
  • Karma: +0/-0
NOT enable signal for screen object
« on: June 23, 2022, 03:41:36 PM »
Maybe I just missed this in the manuals/tutorials. This may belong in the screens forum - sorry if that is the case.

Is here a way to NOT an enable in the screen - so the object shows up when the binary is False? Like entering NOT:wirename in its description of the enable signal.

I realize you can create a new "wire"/variable with a NOT on it and use that instead but it seems clunky.

Thanks in advance.

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: NOT enable signal for screen object
« Reply #1 on: June 28, 2022, 10:10:54 AM »
Hello BBarry,

Unfortunately not.
Today there is Enable TRUE, FALSE and by Signal.  So the best tip is the way you suggested, a NOT component on the signal.

If the idea is not in the wishlist I will add it.  I hope the developers also think it's a good idea.


Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team