Author Topic: DP710 Verify Failed Memory Block  (Read 3341 times)

Offline dloww17

  • PLUS+1 User
  • **
  • Posts: 8
  • Karma: +0/-0
DP710 Verify Failed Memory Block
« on: February 24, 2021, 10:35:23 PM »
I am having an issue with downloading a new ECU value to a memory block in a DP710. Every time I go to download the new parameter on the service tool, I get an error "E245 Verify Failed". I verified that I was editing the correct memory block and had no issues uploading the value. Any help would be appreciated.

Offline Mike AA

  • PLUS+1 Guru
  • *****
  • Posts: 109
  • Karma: +0/-0
    • Dewind Dewatering
Re: DP710 Verify Failed Memory Block
« Reply #1 on: February 25, 2021, 11:41:13 PM »
Are you able to reliably send new programs to the DP710? Have you tried resetting the gateway?

I remember seeing this error a few times but I cant remember what I was doing that caused it and how I fixed it.

Mike

Offline FStelzer

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +8/-0
Re: DP710 Verify Failed Memory Block
« Reply #2 on: February 26, 2021, 08:12:57 AM »
dloww17,

which memory block do you use and do you also write on this NV memory via the software?
I've had this once where I want to change a NV memory value with the service tool but everytime I downloaded the parameter, the software re-writes the parameter and so the error E245 pops up in the service tool.

Regards

Offline dloww17

  • PLUS+1 User
  • **
  • Posts: 8
  • Karma: +0/-0
Re: DP710 Verify Failed Memory Block
« Reply #3 on: February 26, 2021, 04:22:11 PM »
Hi Mike,

I've had no issues with sending new programs to the unit. I recently updated the hardware to v240 and that took quite a bit to download, but I don't think that is unusual.

FStelzer,

I am using an NV memory dynamic component. I do have a page on the DP710 where I can change the value using the buttons and also have buttons assigned for resetting the value to 0.