PLUS+1 User Forum

PLUS+ Tools => PLUS+1 Service Tool => Topic started by: Keithang on May 21, 2019, 08:17:05 AM

Title: Live Updating
Post by: Keithang on May 21, 2019, 08:17:05 AM
Good Day,

I was wondering if it is possible to automatic Input Values into Controller\Display using a CSV File.

Scenario:
I have a Server that is constantly changing values - these values need to be updated on Controller\Display regularly.
Eg. Hole 1 Depth ; Hole 2 Depth ; Hole 3 Depth

Whilst Drilling - the Controller must receive an update from server to say what depth it needs to be at for the required hole.

Is there a way to automate this?

Title: Re: Live Updating
Post by: oiltronic on June 06, 2019, 04:34:40 PM
If I understand correctly, you want a running display to scan a file to receive updated control parameters, correct?

If so, then no, there are no built-in functions to read data from a file while running.  If I had to do this, I would use an Ethernet-to-CAN bridge/adapter and craft a little script sitting on the server or a nearby PC to pull the server and push out a period CAN message.  Then you can use the built-in CAN functions on the display to extract and sanity-check the incoming data.