Author Topic: Red and Green information about all module  (Read 4714 times)

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 115
  • Karma: +1/-0
Red and Green information about all module
« on: April 29, 2022, 03:43:13 PM »
H!

Now I have problem with DM430   red blinking.

I searched in the DM430 API documentation but unfortunately I did not find any information.

Please could you show me where can I find information about red and green of all modules (Display, controller and IO module).

Thank you very much
with best regards
mac bahi

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Red and Green information about all module
« Reply #1 on: May 02, 2022, 11:49:19 AM »
Hi,
Display and Controller, you find in software:
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Red and Green information about all module
« Reply #2 on: May 02, 2022, 11:52:37 AM »
Input, Output modules is if data comes in or out
you can't change this LEDs.
you find it in "Technical documentations"

To simplify system diagnostics the I/O device will use its LEDs, if available, to indicate
different status conditions.
Red LED
The red LED indicates outgoing message traffic from the I/O device. The LED toggles its
state with every successfully transmitted frame.
If the device’s CAN-bus goes into a bus off condition then the LED will be permanently
on.
Green LED
The green LED indicates that the I/O device is seeing incoming message traffic. The LED
toggles its state with every successfully received frame. If no messages are received for
more than 10 seconds, then the LED starts to blink at a one Hertz rate.
Time critical messages and messages which have to be used all the time are
implemented with a sub identifier which has a value from 0 to 0xFE.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Neil

  • PLUS+1 Expert
  • ****
  • Posts: 96
  • Karma: +2/-0
Re: Red and Green information about all module
« Reply #3 on: May 03, 2022, 09:49:54 AM »
If the DM430 red LED's are blinking, and they are not being controlled by your application.
It would suggest you may have an problem with the CAN network?

Increase the two fields in green in the attached png (10, 1000?), download and see if the DM430 reset's itself on the network.

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 115
  • Karma: +1/-0
Re: Red and Green information about all module
« Reply #4 on: May 09, 2022, 04:51:02 PM »
Hello!!

thank you for your replay

sincerely
Mac bahi