Recent Posts

Pages: 1 ... 7 8 [9] 10
81
PLUS+1 GUIDE / Re: Compile error in 2024.1.3
« Last post by Egholm-Jonas on February 26, 2024, 11:38:22 AM »
Hi Camox,

Nothing out of the ordinary!
Except updating to the new Guide 2024.1.3

Yes, I have a 1 month old backup! :'(

If I create a new Application, I does the exact same!
82
PLUS+1 GUIDE / Re: Compile error in 2024.1.3
« Last post by Camox on February 26, 2024, 11:09:17 AM »
Hi, there,
What changes did you make after the previous compilation?
Do you have a backup with the 2023 version of the Guide?

Have a nice day!
83
PLUS+1 GUIDE / Compile error in 2024.1.3
« Last post by Egholm-Jonas on February 23, 2024, 09:42:30 AM »
I see there is some issues with compiling. But only for the display users so far!?
I can't compile on the MC088 either!

On the "error/Warning/Hint messages" tab after 3 seconds of compiling, it shows:
"Completed

 No specific issues identified"

But, on the Build message tab:

"Graphical Compilation and Linking of VCU_SOFTWARE_2XXXX aborted with errors
WARNING: invalid character '0xBB'
WARNING: invalid character '0xBF'
WARNING: invalid character '0xBB'
ERROR: MKFILE11.mak: line 1: needs an operator
?#
^
ERROR: #0210 - 1 error(s) occured while parsing the makefile
84
Controllers / Re: AnIn used as 24vdc DigIn
« Last post by Marbek_Elektronik on February 21, 2024, 09:48:37 AM »
Yes, thanks, indeed.
You are right!
85
Controllers / Re: AnIn used as 24vdc DigIn
« Last post by acmall on February 21, 2024, 08:52:02 AM »
I am not sure , but I think c1p05 at a MC024 controller maximum allowes 25V. All other inputs 36V.

I think the 25V limit on C1P05 is a difference between the MC0xx-0xx controllers and the MC0xx-1xx versions.
86
Controllers / Re: AnIn used as 24vdc DigIn
« Last post by Lukey on February 20, 2024, 11:31:07 PM »
Thanks all,

Yes I will use a comparison block to simulate a DigIn on pin.

My system is a 24VDC regulated switch mode power supply so I don't expect to see anything greater.
According to the hardware manual AnIn pins rated for 36V
87
Controllers / Re: AnIn used as 24vdc DigIn
« Last post by Marbek_Elektronik on February 20, 2024, 04:11:03 PM »
I am not sure , but I think c1p05 at a MC024 controller maximum allowes 25V. All other inputs 36V.
Perhaps you ask helpdesk?
88
Displays / Re: DM1000
« Last post by a.damato on February 20, 2024, 03:28:40 PM »
Thank you very much!
89
Code sharing / Re: J1939 Receiving Large Message (EC, FEE3)
« Last post by nikomas on February 20, 2024, 02:44:14 PM »
Hi,

I have downloaded PLUS+1 GUIDE examples->J1939_Example from Update Centre 1.0.167. and implemented it in order to
receive DM01, DM02, CI and VI messages. Messages are time triggered and sent from PCAN application.
Local address is "5" (DM430 display) and source address "0".
I can receive DM01 and DM02 messages but nothing I can see on RTS_CTS_Msg bus on the checkpoints and on checkpoint after CI_Parse block.
If someone can help I will be very grateful.

Best regards,
90
Controllers / Re: AnIn used as 24vdc DigIn
« Last post by sverreo on February 20, 2024, 09:20:37 AM »
You can use C1p05 without a problem. The only thing is that if you input 24V it will only read maximum 5V on the input.

Make a simple logic to use this voltage as a digital input. f.ex. greater than 3V "on", and less than 2V "off"
Pages: 1 ... 7 8 [9] 10