PLUS+1 Software > Displays
DP710 hwd v240 not compatible
(1/1)
dlewis:
I just had an issue with a couple of DP710 programs with hardware v240. After downloading the programs into the displays the display would not show ANYTHING on the screen. I had this same issue with version prior to 240 but now it's happening again. If I update the program to hdw rev 250, the issue goes away.
BrianF:
dlewis,
You must have a brand new display. They changed the LCDs on the displays and the new hardware version supports that change. I ran into the same problem. If you read the revision history in the What is New section in version 250. You can get a clue to what changes have been made by Danfoss.
I make a habit to watch which downloads the update center offers. If one of the hardware files is updated for a module or display that I use, I try to read the revision history file. It gives me a little bit of a warning that something is about to change. Sometimes it is just a bug fix and I don't have to do anything, other times I know I need to get a new version of the software ready with the updated hardware file.
I have been caught off guard a few times and had to make emergency builds because a machine went down and we had to replace a module and the replacement was one of the "new and improved" modules.
Navigation
[0] Message Index
Go to full version