Author Topic: how to monitor the system value  (Read 4973 times)

daifuku chan

  • Guest
how to monitor the system value
« on: June 20, 2011, 03:56:59 AM »
Which botton to monitor the system?And read the value of the output?  THANKS   :-\ :-\

Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 98
  • Karma: +2/-0
Re: how to monitor the system value
« Reply #1 on: June 20, 2011, 08:30:32 AM »
The "hotkey" for those functions are shown in the dropdown menu's at the top of the screen.
Start logging = F5

Scan connected system = F8

Upload parameters = F2       (Read parameters from ECU)
Download parameters = F4   (Write parameters into ECU)

Im not sure if this answers your question, tho.