Author Topic: Missing fonts error when trying to compile with 2024.1  (Read 5542 times)

Offline williamk

  • PLUS+1 Developer
  • ***
  • Posts: 21
  • Karma: +1/-0
Missing fonts error when trying to compile with 2024.1
« on: February 13, 2024, 12:54:42 AM »
I have a project that I can successfully compile using version 2023.2, but when I try to compile it in 2024.1 I get the following error message:

*** ERROR 597 *** [PLUS1_IDE] Screen Editor Error: {Error Code201; Missing fonts:
Balboa ExtraCondensed [Bold]
Franklin Gothic Book [Bold]
Franklin Gothic Demi [Bold]
Franklin Gothic Demi Cond [Bold]}

I've tried uninstalling and reinstalling the font, but that hasn't fixed the issue.

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 287
  • Karma: +28/-1
Re: Missing fonts error when trying to compile with 2024.1
« Reply #1 on: February 13, 2024, 09:05:58 AM »
Hello williamk

I will post the same thing as I posted in another thread with the same issue:

"Yes, there seems to be a bug when it comes to some fonts and this is reported. I hope they can find a a solution quickly, and I guess, get a patch out.

Sorry about the inconvenience."



Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline williamk

  • PLUS+1 Developer
  • ***
  • Posts: 21
  • Karma: +1/-0
Re: Missing fonts error when trying to compile with 2024.1
« Reply #2 on: February 13, 2024, 05:28:52 PM »
Ah, I looked quickly before posting and didn't see that post.  Thanks for the reply.

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 287
  • Karma: +28/-1
Re: Missing fonts error when trying to compile with 2024.1
« Reply #3 on: February 14, 2024, 08:28:50 AM »
Hello williamk,

Sorry, I didn't mean that you should know what I have commented in another thread.  The comment "..the same thing in another thread...." was just to inform that more people had the same issue.   :D


Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline williamk

  • PLUS+1 Developer
  • ***
  • Posts: 21
  • Karma: +1/-0
Re: Missing fonts error when trying to compile with 2024.1
« Reply #4 on: March 06, 2024, 06:08:52 PM »
This appears to be fixed in 2024.1.4