Author Topic: PVEA Compliant Block  (Read 6105 times)

Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 103
  • Karma: +2/-0
    • Getman Corporation
PVEA Compliant Block
« on: February 04, 2011, 07:29:53 PM »
I've been using PVG32 valves with PVEA coils for years.  To control them with the Plus+1, i've been using the PVE Driver block from the Library.

I thought I'd try something different and tried to use the PVEA_H_S Compliant Block from the HWD file, but when I try to compile, I get a bunch of errors.

*** ERROR 21 ***  [CHPARGU2]   NO OUTPUT CONNECTED TO COMPONENT: {AND2}, ENTRY A2
          MC50_10T_MC50_12T!TOP!Application!BASIC!PVE_A_H_S1!PVEA_H_S!PVE_Driver!PVE_Driver (348,220)
*** ERROR 21 ***  [CHPARGU2]   NO OUTPUT CONNECTED TO COMPONENT: {Switch 2}, ENTRY A3
          MC50_10T_MC50_12T!TOP!Application!BASIC!PVE_A_H_S1!PVEA_H_S!SupplyHandling (352,162)
*** ERROR 98 ***  [CHPARGU2]   INVALID MIX OF INPUT AND OUTPUT TYPES FOR COMPONENT: {Switch 2}
          MC50_10T_MC50_12T!TOP!Application!BASIC!PVE_A_H_S1!PVEA_H_S!SupplyHandling (342,150)



Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 103
  • Karma: +2/-0
    • Getman Corporation
Re: PVEA Compliant Block
« Reply #1 on: February 04, 2011, 08:29:41 PM »
I found the problem, my enable signal wasn't getting through.