Author Topic: J1939 DM1 and DM2 messages  (Read 9409 times)

Offline tjozmin

  • PLUS+1 Developer
  • ***
  • Posts: 10
  • Karma: +0/-0
    • Oxbo International Corporation
J1939 DM1 and DM2 messages
« on: April 07, 2011, 09:55:08 PM »
Has anyone built a block to receive engine faults? I know the EIC applications does this but I find this is mostly for a display that is dedicated to engine monitoring. The software has quite a bit of code that I have no use for.

payne.byron

  • Guest
Re: J1939 DM1 and DM2 messages
« Reply #1 on: April 11, 2011, 08:19:49 PM »
There are some blocks in the Function Library that can help with this. I as well started out using the EIC application, and then redesigned using the function blocks.  Download the J1939 library here:

http://www.sauer-danfoss.com/Products/MobileElectronics/PLUS1Guide/PLUS1GuideDownloads/PLUS1FunctionBlockLiabrary/index.htm