Recent Posts

Pages: [1] 2 3 ... 10
1
Controllers / Re: MC018 C1p11 error 23 and 665
« Last post by macbahi on May 08, 2024, 02:31:45 PM »
Hello Fitz

Thank you very much to answer me.
The error it's was feedback but plus+1 compiler show other thinks.
Since I installed the last version the compilation it's not as before.

Any way thanks sir.

With best regards
mac bahi
2
Controllers / Re: NV Memory writing error
« Last post by federico.furlani on May 08, 2024, 11:13:44 AM »
Exact version is 2024.1.3.5743.

Do we need to update our installations?
3
Controllers / Re: NV Memory writing error
« Last post by Camox on May 07, 2024, 01:32:25 PM »
Hello,
What is your exact version?

Version 2024.1.4 had a memory problem.
Here is an extract from the Guide release notes:
Version 2024.1.4
2024.1.4 (February 2024)
What is Fixed
[P100006950] Some fonts were incorrectly reported as missing.
[P100006939] In some cases, an application containing images would not compile.
[P100006956] NV memory writes


Have a nice day
4
Controllers / NV Memory writing error
« Last post by federico.furlani on May 07, 2024, 11:01:37 AM »
Hi all,
I'm facing an error in memory writing.
It seems that with the new version, 2024.1, an original logics part, migrated from 2023.3, that has no problem, started with writing error.
If I reduce the logics with this memory handling, is seems ok.

If I write this memory from Service Tool, it is ok. If I write this mem from logics, it takes the previuos value at power cycle.

Ideas?
5
General controls / Re: HINT 4000 DISABLE
« Last post by Mike AA on May 06, 2024, 11:15:12 PM »
Figured it out myself. Once again, search the help. In the options there is a setting to de-select the hints.
6
Controllers / Output Configured for both/either Sinking or Sourcing
« Last post by Lukey on May 05, 2024, 08:58:04 AM »
Is it possible for an output to function as both Sinking and Sourcing?

I successfully test complied an application that changes the Output mode from 1 to 2 during runtime of the controller.

I took examples from this topic https://www.plus1forum.danfoss.com/index.php?topic=1525.0

By setting my INIT hardware output to constant 1 / sourcing

Then used a switch to change the pin OutputMode from 1 to 2 with an bool signal.

Does the output hardware physically allow this to function as intended/programmed? is there any risk to damage?
7
Communication / BUS Load - CANOpen vs J1939
« Last post by Lukey on May 04, 2024, 02:18:11 AM »
Typically which protocol generates more bus load? Within a system of lots of nodes?

Often when selecting hardware like JS1H joysticks, PVE CAN coils and other Danfoss sensor there is always both options CANOpen Or J1939.

Almost all my applications are using a GUIDE controller so there is no limitations there, I'm not concerned about the pros or cons of each protocol but concerned when designing a system with lots of nodes/devices, which would be best to select to reduce bus load?
8
General controls / HINT 4000 DISABLE
« Last post by Mike AA on May 03, 2024, 11:26:50 PM »
I use value connect in my programs for a lot of selection stuff. It seems whenever there is an error I get a Hint 4000 that talks about the value connect code change

*** HINT 4000 *** [CHPARGU2] Code generation has changed for component {Value} since version {2022.1} due to {P100005975}. Note that this only points out where the code has been changed, it does not necessarily mean that that code was affected by any problem.

Is there somewhere I can disable this? Am I doing something wrong with the value connect components? It gets maddening scrolling through 29? errors that aren't errors to find one connection I missed somewhere.
9
Displays / RTC GNSS TIME updated
« Last post by Mike AA on May 02, 2024, 09:39:56 PM »
I recently found out I can sync the DM1200 clock with GPS by just enabling GNSS and connecting a GPS receiver antenna. Now that I know that the time is perfect I wish to get info that it has indeed synced which according to the API I can use RTC.Auto, atleast I think I can, to light up an indicator. I need this to work with our Trimble GPS sytem for DATA logging and machine logging. I have a setup where the Danfoss computer trips a relay which acts like a button push on the Trimble system to create a point.

I cannot find on the RTC bus the .Auto element which the API says is there. Has anyone used this function or have an idea how to read the .Auto data?
10
Controllers / Re: MC018 C1p11 error 23 and 665
« Last post by A.Fitz on May 02, 2024, 04:50:17 PM »
It looks like nothing is connected to the DigOut component based on the error.
I would use command "V" to view the connection and verify you have something driving it.

I would bet this is a copy paste error where you forgot to change the name somewhere to correlate to this pin.
Pages: [1] 2 3 ... 10