Author Topic: Search/Replace Signal Names [Resolved]  (Read 8626 times)

Offline PatrickS

  • PLUS+1 User
  • **
  • Posts: 6
  • Karma: +0/-0
Search/Replace Signal Names [Resolved]
« on: January 18, 2021, 08:44:33 PM »
I'm working on updating a program and have decided that some of our old signal names should be changed to be more descriptive.
I've found the Search/Replace dialog within Plus +1 and the Search functionality works fine. However; I cannot get the Replace functionality to work at all. To me it looks like that the main issue is all replaceable item checkboxes are greyed out, so when i go to update the replacement list I just get the message 'There are no items to replace checked'.

Am I missing a setting somewhere or is this functionality just not available?

« Last Edit: February 08, 2021, 05:03:05 PM by PatrickS »

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 201
  • Karma: +37/-1
Re: Search/Replace Signal Names
« Reply #1 on: January 19, 2021, 09:35:23 AM »
If I remember correctly the Replace functionality is only available for the Vector Based Screen Editor.






Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 296
  • Karma: +28/-1
Re: Search/Replace Signal Names
« Reply #2 on: January 19, 2021, 09:38:42 AM »
Hi PatrickS,

I'm sorry to say that the Search & Replace function only works for items in the Screen Editor for now.  So if you open a display application the boxes won't be grayed out.
I believe it's because of some limitation within the CAD engine that is used for GUIDE, and as far as I know the developers are working on it.

This is something that could/should be stated in the manual.

Have a nice day

(Edit: acmall was quicker than me.)
Best regards,
Tor
PLUS+1® SW PAE Team

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 296
  • Karma: +28/-1
Re: Search/Replace Signal Names
« Reply #3 on: January 20, 2021, 08:32:11 AM »
Hi PatrickS

I was a little bit unclear in my post. 
I can't find it in the manual either, but it is something that should be stated in there.  I will point this out to the responsible people.

Thanks for letting us know.

Have a nice day
Best regards,
Tor
PLUS+1® SW PAE Team

Offline spittet

  • PLUS+1 Guru
  • *****
  • Posts: 118
  • Karma: +6/-1
Re: Search/Replace Signal Names
« Reply #4 on: January 25, 2021, 11:10:49 PM »
You can change the name of a signal by using the tool "Change Port Names across Pages" while you are inside the "View Logical Net" tool ("v" touch shortcut on the keyboard).

Sam