PLUS+1 Hardware > PLUS+1 Compliant Hardware
Joystick JS7000 (CANopen)
(1/1)
andrzey13:
Hello,
I have got questions about joystick JS7000.
It works on NODE iD = 10 and baudrate = 250kbps
The problem is that joystick does not transmit frames about his axis X and Y and buttons itself.
But, when I transmit a command directly to joystick to force it, he starts transmit.
My commands:
60A 8 40 01 64 01 00 00 00 00 – cyclic 10ms (force respond from axis X)
60A 8 40 01 64 02 00 00 00 00 – cyclic 10ms (force respond from axis Y)
60A 8 40 00 60 02 00 00 00 00 – cyclic 10ms (force respond from buttons)
In my opinion it looks like the joystick needs an event to transmit his data.
Maybe there is a command which can change this behavior from event to cyclic sending.
Is there a command to set default settings, maybe hard reset?
Navigation
[0] Message Index
Go to full version