PLUS+1 User Forum

PLUS+1 Software => Displays => Topic started by: Rafal_Typiak on November 16, 2010, 12:55:12 PM

Title: Encoder problem
Post by: Rafal_Typiak on November 16, 2010, 12:55:12 PM
Hello,
I'm having a problem with checkpointing an encoder input in a DP600. I connect a DigIn_c1p09 to a simple checkpoint block and after compiling I get an error: 'SIGNAL TYPE NOT DEFINED FOR: Simple Checkpoint'. Could someone tell me what's wrong?  And the same thing happens to every onther checkpoint I connect to the encoder inputs.

p.s.
I just noticed the same thing happens when I connect a checkpoint block to ANY input. What the hell?
Title: Re: Encoder problem
Post by: Quax76 on November 16, 2010, 01:30:05 PM
Hi,

I think, I know what you mean. PLUS1 seems to have a problem with connecting a checkpoint to any port, which you can see in the Service Tool (HW_In; EEParameters; etc.)
In my cases it worked, when putting any throughpassing component(e.g. bool switch or value connect) between the input and the checkpoint.
Title: Re: Encoder problem
Post by: slewis on November 17, 2010, 04:48:58 PM
Try connecting a "Predefine Type" component to the signal (found in the Manage section).  It defines a data type for signals that don't already have one.
Title: Re: Encoder problem
Post by: Federico on November 17, 2010, 06:43:16 PM
Hola,
TambiƩn puedes colocar el bloque RETYPE (BOOL) entre el Checkpoint y DigIn,
RETYPE esta en Data Conversion
Saludos Cordiales.

Hello,
You can also place Retype block (BOOL) between Checkpoint and DigIn,
Retype this in Data Conversion
Best regards.