Recent Posts

Pages: 1 [2] 3 4 ... 10
11
PLUS+1 Service Tool / Downloadable File not Updating After Saving Project File
« Last post by swilkins3 on September 27, 2023, 02:58:32 AM »
Hello,

Lately, I have been making changes to some code for an old DP600 Display. In the past, I have had no issues updating the code, uploading it, and debugging by viewing checkpoints on the service tool. Just recently, though, I have tried uploading updated code and I'm not seeing my changes reflected on the display or in service tool. While uploading the code, everything behaves as it always has in the past.

When I look at the files in my file explorer, I have noticed that the date modified for the SCS file seems correct (Sept. 26- consistent with my most recent code changes). However, my Plus+1 Downloadable File that is typically uploaded to the display through the service tool has a date modified of Aug 27th. Additionally, my Plus+1 Project File has a modified date of July 30th, even though I just made changes to it in Guide today (Sept. 26th). I'm rather unexperienced with Guide, but I suspect my problem is that the files I mentioned are not synced correctly. How can I get them to sync correctly? Or could something else be causing the upload to not work correctly?
12
Controllers / Re: Using MC024 to control s20 pump
« Last post by Mr.Jacobee on September 26, 2023, 08:30:08 AM »
Thank you guys very much ;)
13
PLUS+1 Compliant Hardware / Re: MPCAN Receiver for IK2 Transmitter
« Last post by Lukey on September 26, 2023, 06:05:24 AM »
Yes the CAN mapping documentation should have been supplied with the RCT system, alternatively you could use CAN king to determine each signal manually.

There is no straight mapping documentation as every system is unique.

Are you using the system with a Danfoss Controller? If so it's much easier to use the PLUS+1 compliance block, although this feature needs to be enabled by whoever supplied the RCT system.
14
Controllers / Re: Using MC024 to control s20 pump
« Last post by Lukey on September 26, 2023, 06:00:01 AM »
If using the S90 EDC block then yes you can change the max current to 100mA, changes are made in the Config_data page of the compliance block.
15
Controllers / Re: Read multiple Can messages same ID
« Last post by FluidPowerTom on September 25, 2023, 05:14:06 PM »
What I entered wasn't really intended as for copy paste.  There are at least one or two errors.  It was more intended as an example to understand and potentially pull from if desired.
16
Controllers / Re: Using MC024 to control s20 pump
« Last post by FluidPowerTom on September 25, 2023, 05:12:46 PM »
You can control current as high as you like up to 3,000 mA on most outputs.  I'm not sure if you'd do this by changing a setting in the S90 compliance block or by just making your own code, but either way I think it'll work fine.
17
PLUS+1 Compliant Hardware / Re: MPCAN Receiver for IK2 Transmitter
« Last post by jtica on September 25, 2023, 04:38:24 PM »
The CAN mapping documentation should have been included with the IK2 and MPCAN system.
18
PLUS+1 Compliant Hardware / PVED-CC S5 ISOBUS
« Last post by jtica on September 25, 2023, 04:29:12 PM »
I am having no luck in connecting to PVED-CC S5 ISOBUS coil in service tool with the PVED-CC S5 ISOBUS P1D file.
When it does the system scan, the ECU shows as 0,32 - S5_TR_APP and status E553: No Diagnostic Data file installed.
I tried changing the ECU, but there are no other selection on the replace with drop down menu.
I just need to change the Node ID to something else.
19
PLUS+1 Compliant Hardware / Re: Adapting PVED-CC seris 4 valves to series 5?
« Last post by jtica on September 25, 2023, 03:28:35 PM »
Hello ardatanikyan,

I am currently having the same issue right now. The link you provided does not work anymore.
Could you please provide another link so I can change the node on my coil?
20
Controllers / Using MC024 to control s20 pump
« Last post by Mr.Jacobee on September 25, 2023, 02:05:51 PM »
Hello,

Could anyone tell me if it is at all possible to use PLUS+1 software to control pumps like those from s20? Better yet, is there any way to change output current on a pin ? Let's say I use standard s90 EDC block in GUIDE and I want to get it to 100mA (while standart for EDC on s90 should be 85mA)?

Thank you all in advance.
Pages: 1 [2] 3 4 ... 10