Author Topic: Sc024-120 output mode with floating  (Read 10496 times)

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 129
  • Karma: +1/-0
Sc024-120 output mode with floating
« on: October 30, 2024, 07:03:02 PM »
Hello,

Please I need more information about output mode 0, 1 2 and 7.

Output mode 0 is push/pull  so if DigOut is set to 0 the output will be GND
                                              if DigOut is set to 1 the output will be Vcc

Output mode 1 is push/pull  so if DigOut is set to 0 the output will be Floating signal.     Are you agree????
                                              if DigOut is set to 1 the output will be Vcc


Output mode 2 is push/pull  so if DigOut is set to 0 the output will be Floating signal or GND?   I am not sûre what is?
                                              if DigOut is set to 1 the output will be GND.

Mode 3 is not is not clear for me when The output is set logic 0.   The outpout is foating or GND.

Concerning output mode 7 I never use it. Please Could you give more information with schematic will be more appreciated.

I need when an output  when is OFF, The output is floating and when the Output is ON the Output will be GND.


Thank you very much.


With best regards