Hello,
News about the issue:
"There is currently a problem with our Danfoss Identity Provider (DIP).
This issue is currently preventing all login attempts through the PLUS+1 Update Center. Therefore, you should currently refrain from logging out of the PLUS+1 Update Center, as a later attempt to log in will not work.
This issue currently affects the PLUS+1 Update Center and Remote InterLink login via PLUS+1 Service Tool.
The issue has been identified and fixed, and a patch will be released as soon as possible for the Update Center and the Service Tool.
Please contact the helpdesk if you need data, documents, or other attachments that you normally receive from the PLUS+1 Update Center."
There is also a "work around" identified. - Note! This didn't work for me, but for some of my colleagues - :
"Without closing the White popup window if you right click on the icon in the task bar you can open the PLUS+1® Update Center window. See image.
When this window is open (It will indicate there are no subscriptions ) if you press F5 the software looks like it is scanning the subscriptions, there is a “hide” button that needs to be pressed.
This closes out the Update Center window and you get a popup indicating the PLUS+1 Update Center is still running.
If you then again right click on the icon in the Windows Task bar (this icon remains in spite of the previous popup) it looks like the subscriptions are now populated."
I hope it helps some of you. If not, I hope the patch will be released soon.
Have a nice day.