Author Topic: Insert wire and bus ports  (Read 4282 times)

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Insert wire and bus ports
« on: October 02, 2020, 01:56:24 PM »
Hi,
I place a port in Guide page interface editor, OK.
If I want to place a second port, I can't edit the name while I am placing it.
Is there a key combination?

Today I place the second port an press "Esc" and then press "Q" and then edit this last port.

Is there a trick?
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 278
  • Karma: +27/-1
Re: Insert wire and bus ports
« Reply #1 on: October 05, 2020, 09:02:08 AM »
Hi Marbek_Elektronik,

I see what you mean, you would like to have the "Entry attribute" pop-up every time you place a port, and not every time you click "Wire/Bus Port"?
Now it adds a number to the end of the name you choose for the first one, like port, port1, port2 and you need to manually change the name.
I believe that you usually have different names on ports, so it would be logical to have the attribute pop-up every time you place the port.  I will ask the developers about this.

What you can do is clicking the "Wire/Bus Port" button every time, then the attribute pop-ups before you place it. You don't have to press "Esc" until you are done.

Have a nice day.

« Last Edit: October 05, 2020, 09:38:30 AM by Tor »
Best regards,
Tor
PLUS+1® SW PAE Team

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Insert wire and bus ports
« Reply #2 on: October 05, 2020, 02:48:15 PM »
Yes, thanks.

Another thing is placing constants:
It would be very nice, if the value popups after placing it.
At the time, I place it and then type "Q" and edit it.

Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 278
  • Karma: +27/-1
Re: Insert wire and bus ports
« Reply #3 on: October 06, 2020, 08:07:32 AM »
Hi,

I had the "constant" discussion with my colleague as well and I will absolutely bring this up.


Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team