Author Topic: Text not formatting properly  (Read 7029 times)

Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 103
  • Karma: +2/-0
    • Getman Corporation
Text not formatting properly
« on: January 25, 2017, 03:22:08 PM »
I'm using a DP710 and Guide 9.0.7.  I'm having an issue with text formatting properly on the display screen.  When I view the text within Guide, it shows the proper formatting, but when I compile and download it to the display, the display does not have the same format.  I don't remember having this issue in previous versions of Guide.

Offline oiltronic

  • PLUS+1 Guru
  • *****
  • Posts: 170
  • Karma: +15/-0
Re: Text not formatting properly
« Reply #1 on: January 25, 2017, 11:22:33 PM »
What aspect of the format is incorrect?

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: Text not formatting properly
« Reply #2 on: January 26, 2017, 03:14:49 PM »
Hi dlewis!

What is your setting for the screen resolution on your computer? Having e.g. it set to 125% at compilation in GUIDE could give this behaviour after download to a display. There actually is a requirement in the Release notes for GUIDE that you need to use Display/text size set to 100% at all times.

Best regards
Nilla
PLUS+1 Helpdesk

Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 103
  • Karma: +2/-0
    • Getman Corporation
Re: Text not formatting properly
« Reply #3 on: January 27, 2017, 03:51:08 PM »
It is removing blank lines between text lines. In another instance, it combined multiple lines into one.  My screen is at 100% with a resolution of 1920x1080.

Offline Nilla

  • PLUS+1 Guru
  • *****
  • Posts: 253
  • Karma: +13/-0
Re: Text not formatting properly
« Reply #4 on: January 30, 2017, 11:13:40 AM »
Hi dlewis!

I've done a simple application for a DP710 adding some text with blank lines as both a simple text and also in a text list, see attached, but I'm not able to replicate what I think your issue was based on what you stated above. Tried out a blank line both with and without any space on it. Would you be able to send us your application in a .P1P-format to plus+1helpdesk@danfoss.com so I can have a look at it and trying to download it on my testbench?

Best regards
Nilla
PLUS+1 Helpdesk