Author Topic: how to Copy (export) screen pages from another scs-file with 7.1 version  (Read 5366 times)

henrisavey

  • Guest
I read in Plus+1 guide 7.0 released
"new features and options include:
- the capability to import and export display screens
- rescale sreens".

Can-you explain how we can do that exactly ?
Is-it possible to do that between DP200 and DP570 ?

Cordially

Henri
« Last Edit: January 13, 2015, 03:46:00 PM by henrisavey »

Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 98
  • Karma: +2/-0
Re: how to Copy (export) screen pages from another scs-file with 7.1 version
« Reply #1 on: January 14, 2015, 11:30:13 AM »
I would say no, you can not export a screen from a DP200 to a DP570, because the DP570 uses the Vector based screen editor (Show screen function) where the DP200 uses the classic (Define area/Define Screen functions).

But the export/import actually seems fairly straight forward, just open the left side panel (Project manager) and look for the screen definitions folder. Right clicking this will show the option to export or import definitions.

I hope this clarifies a few things for you :)

regards Jakob

radioact

  • Guest
Re: how to Copy (export) screen pages from another scs-file with 7.1 version
« Reply #2 on: February 15, 2015, 07:16:17 AM »
It will be handy going forward but I think you are in the same spot I was; you will have to redraw all your screens in the vector screen editor. You can copy the code over but that's about it.