PLUS+1 Hardware > Controllers
Real-time clock.
ET:
Is there a real-time clock component in GUIDE?
I want to put a screen on a DP600 (which is connected to an MC050-010), which will keep track of daily/weekly/etc miles paved.
I already know how to get the time since the unit was powered on.
However, I can't seem to find any components in GUIDE, which would read, or set, the current time in human units, and keep track of it while the machine is powered off.
e.g. Year, month, day, hour, second.
Where is this functionality?
Quax76:
This is quiet simple.
There is no component in Guide itself.
The templates of components which has a RTC has an RealTimeClock Bus on the Input Bus.
ET:
I'm sorry, I didn't understand what you said.
Is there a real-time clock on Sauer Danfoss controllers, or is there not?
(For example, an MC50-010.)
If there is, how do I access it?
Jakob:
I only seen the RealTimeClock on the displays.
A RTC on a MC controller would be great.
So far I have made a counter function to keep track of machine running hours, unless the system included a display.
The memory of the display would also be better suited to keep track of all those data.
Richard:
I don't think many people know this but in the Inverter Function Block Library there is aready made hour counter along with several other function blocks.
Navigation
[0] Message Index
[#] Next page
Go to full version