Author Topic: Graphics Software  (Read 4672 times)

Offline tjozmin

  • PLUS+1 Developer
  • ***
  • Posts: 10
  • Karma: +0/-0
    • Oxbo International Corporation
Graphics Software
« on: February 08, 2012, 01:00:53 PM »
What software works the best for developing the graphics? I have heard people start with their CAD software and then convert it to a bitmap. I tried that but I have trouble getting the sizing right. I have tried Paint but that just seems be difficult to do any shading.

Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 102
  • Karma: +2/-0
    • Getman Corporation
Re: Graphics Software
« Reply #1 on: February 08, 2012, 01:10:31 PM »
I use CorelDraw.  It's a vector based graphic program.  Once I create the graphic in coreldraw, I export it as a bitmap to the exact size I require.

Offline 240glt

  • PLUS+1 Developer
  • ***
  • Posts: 35
  • Karma: +0/-0
Re: Graphics Software
« Reply #2 on: February 09, 2012, 11:15:39 AM »
I use Inkscape. It's open source, and free. Vector-based. Should be similar to corel draw.
http://inkscape.org/

For bitmap editing, i use gimp. Also open source, free to use.
http://www.gimp.org/

For viewing pictures, and for simpler image manipulations, like changing size, compression, cropping etc. I use XNView.
Free for personal use. Very fast, and a lot nicer than windows integrated viewing utility.
http://www.xnview.com/