Author Topic: Widget library keypad  (Read 1732 times)

Offline macbahi

  • PLUS+1 Expert
  • ****
  • Posts: 87
  • Karma: +1/-0
Widget library keypad
« on: January 15, 2021, 03:12:27 PM »
Hi

I use widget library keypad.  The problem is when I touch any number one time the result is the number repeated 9 times as showing in picture included

Please Can you help.

Thanks in advance
 

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 204
  • Karma: +4/-0
Re: Widget library keypad
« Reply #1 on: January 15, 2021, 10:36:51 PM »
mm I did not know there was a widget for the numeric pad.

anyway, check the time setting for the touch screen, see picture.

Most of the times what comes as default values work well, I did my own numeric pad so I had control on the logic and it did work fine

hope it helps


Offline macbahi

  • PLUS+1 Expert
  • ****
  • Posts: 87
  • Karma: +1/-0
Re: Widget library keypad
« Reply #2 on: January 19, 2021, 06:34:34 PM »
H!

Thank you very much for reply but without effect

Cordially