PLUS+1 Hardware > Controllers
SC050-120 configurable dig out
Beezkneez:
I see in the datasheet for the SC050-120 controller that the 6 DigOuts are configurable between sink/source. I have not been able to find where I can ensure that they are set to sourcing. Has anyone done this before? I searched the template and didn't find a setting there.
I see the datasheet is dated 2014, so I am also wondering if that is out of date. If that is the case, are the dig outs "sourcing only" similar to the MC050-110?
Thanks,
Jake
jashom1:
Hi Jake,
That's set in the outputs page for the individual output pin.
Also MC050-110 can be configured as sinking or sourcing too!
Cheers,
John.
Beezkneez:
Hi John,
Thank you for the reply. The pins of concern for me are 33-38 DigOut only. Since the datasheet states 6 DigOut configurable as Sink/Source and 8 PWM, and there is a total of 14 outputs, I assumed the datasheet was talking about the 6 DigOut only pins were configurable. I am using the PWM capability of pins 39-46.
Thanks,
Jake
jashom1:
Hi Jake,
My misunderstanding! I'd say the brochure must be a miss-print as the digital outputs are definitely sourcing only.
Cheers,
John.
Beezkneez:
Awesome, thank you for the info!
Jake
Navigation
[0] Message Index
[#] Next page
Go to full version