PLUS+1 User Forum

PLUS+1™ Hardware => I/O Modules => Topic started by: bryantmorris on July 08, 2016, 07:02:31 AM

Title: IO024 CAN Error
Post by: bryantmorris on July 08, 2016, 07:02:31 AM
Hello,

I'm working with a SC050-010, a OX024 and 2 IX024 expension modules in a plus+1 program. I'm now getting an error regarding the CAN_Out subpage which I can not access. The error is as below:

The CAN Port on the module is connected, any idea what could be causing this issue?

Title: Re: IO024 CAN Error
Post by: Jakob on July 08, 2016, 08:45:26 AM
Hi,
Don't use - in the Outputmodule bus name, but use _ instead.

For example, do not write OX024-010, but do write OX024_010.

I had this one too once or twice.
/Jakob