PLUS+1 User Forum

PLUS+1 Tools => PLUS+1 GUIDE => Topic started by: ET on September 21, 2012, 12:26:46 AM

Title: BUG: Compilation aborted with error(s).
Post by: ET on September 21, 2012, 12:26:46 AM
Sometimes, when I compile an existing program, the compiler window stops with "Compilation aborted with error(s)., but when I press OK, the error message box at the bottom of GUIDE is completely empty.
If I compile the program a second time, it works without any problems.

This usually only happens when I compile an existing program for the first time after re-opening it.
It happens with programs for MC50s, DP200s, and DP600s.
Title: Re: BUG: Compilation aborted with error(s).
Post by: Quax76 on September 21, 2012, 08:00:09 AM
I knew this problem, too. There is no error listed in the compiling window. This is pretty unfine...
This phenomenon also occurs. when I add an image to an excisting project an the name of the file contains 2 spaces in a row.
Title: Re: BUG: Compilation aborted with error(s).
Post by: Jakob on September 21, 2012, 09:16:17 AM
If the lhx readme file is open, it also stops the compilation with a blank error window.
But in that case it does write the cause of error in the build window.