PLUS+1 User Forum
PLUS+1 Tools => PLUS+1 GUIDE => Topic started by: paterianus on July 19, 2011, 10:28:42 PM
-
If I download a new hwd file from the S-D web site are the new feaures automatically included the next time I compile a project or am I required to manually delete and re-install the associated hardware?
-
You need to change the HWD file in the application manually.
First you need to install it in GUIDE. Go to setup/install hardware then you see it appear in the Hardware tab on the right. Then either drag the sys file from the right to the project manager tab/sys file on the left or right click on the new hardware file and select 'use this hardware in project'.
Hope this helps.
Richard
-
Do you prefer to use the newest HWD-File (sys-file) by opening a project in a new Guide version?
I want to open older projects from Guide 5 and I want to do some changes.
One way is to import the project an do the changes.
The other possibility is to change the sys-file at first. Could this produce new errors?
Is it better to change the sys-file?
Bye
Bernd Konrad
Marbek Elektronik
(Germany)