PLUS+1 User Forum

PLUS+1™ Software => Communication => Topic started by: SunnyMan on September 03, 2018, 09:56:25 AM

Title: TTL Serial Communication
Post by: SunnyMan on September 03, 2018, 09:56:25 AM
Hello,

we would like to convert the TTL serial signal of distance (ultrasonic sensor) to a MC012 Controller. Do anyone know or do anyone has experience how we can do it?

We can use a converter TTL/CAN, but I will try to connect it directly as our first step... if it possible, of sure :)

Thanks for any idea how to do it.

PS. The description of data of TTL protocol is attached.

Best regards

Michael
Title: Re: TTL Serial Communication
Post by: Marbek_Elektronik on September 04, 2018, 05:37:02 AM
Only Controller with RS232 are Displays DP6xx and DP7xx and ....
MC012 can't do RS232.

What is the distance between sensor and Controller?
RS232 with 9600bit/s is to fast to handle without RS232-interface in controller.
If you wand to handle this manually, the bit-rate should be very slow.

I think, the best way is, to convert it to can-signal.