Author Topic: ERROR 131 with CHECKPOINT Box  (Read 3654 times)

Offline bryantmorris

  • PLUS+1 Expert
  • ****
  • Posts: 51
  • Karma: +0/-1
ERROR 131 with CHECKPOINT Box
« on: April 28, 2016, 08:16:18 AM »
Hello all,

I'm getting the following error when trying to attached a CHECKPOINT to a variable. I am able to attach the item however when I try to define a name I get the following error (see attached). It doesn't matter what I call the variable I get the same error. The variable type is BOOL if that matters at all.

ERROR 131 *** [PLUS1_IDE] INVALID SIGNAL NAME {>t<}

In this situation I had used the name 'test" but it seems to have only looked at the first letter. It did the same for whatever name I used.

Any help you could provide on what may be causing this would be appreciated.

Offline Loader

  • PLUS+1 Expert
  • ****
  • Posts: 50
  • Karma: +3/-0
  • If something can go wrong, it will!
Re: ERROR 131 with CHECKPOINT Box
« Reply #1 on: April 28, 2016, 08:25:19 AM »
Hallo Bryantmorris,
if I right remember, the first letter must be uppercase!
bye

Offline bryantmorris

  • PLUS+1 Expert
  • ****
  • Posts: 51
  • Karma: +0/-1
Re: ERROR 131 with CHECKPOINT Box
« Reply #2 on: April 29, 2016, 03:36:06 AM »
Thanks Ill give that a go